Set up how the DeskLock System Restart button looks (Appearance tab)

Use the
Properties
dialog box to set up how the
DeskLock System Restart
button looks.
To set up the appearance options for the DeskLock System Restart button
  1. In the
    Graphics Display
    editor, double-click the button to open its
    Properties
    dialog box.
  2. Click the
    Appearance
    tab.
  3. Specify these properties:
    • Caption text, font, size, style and color
    • Caption text background color
    • Image
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal