DeskLock System Restart button Appearance tab options
The following table shows the options on the
Appearance
tab in the DeskLock System Restart Button Properties
dialog box.Options | Descriptions |
|---|---|
Caption | In the text box, specify the text for the button. By default, the button's caption is DeskLockSystemRestartButton1 . The text appears on the face of the button, and changes color when the button is pressed to enable or disable the hot key sequence specified in the General tab. |
Font | Select the font to use for the caption. |
Size | Select the font size to use for the caption. |
Bold, Italic, Underline | Select a font style for the caption, if required. |
Background color | This box shows the current background color for the caption. Click it to select another color. |
Image | Click the Browse button to open a standard search window. Navigate to the desired image and click Open . The image appears on the face of the button at runtime.To remove the image from the button, click Clear . |
Provide Feedback