DeskLock System Restart button General tab options
The following table shows the options on the
General
tab in the DeskLock System Restart Button Properties
dialog box.Options | Descriptions |
|---|---|
Restart | Shut down and restart the operating system |
Shutdown | Shut down the operating system. |
Force processes to end | Select this check box to force all applications to close. |
Provide Feedback