DeskLock
DeskLock is a
FactoryTalk View
tool for the Windows operating system.
IMPORTANT:
FactoryTalk View
has enhanced the security of the utility. We strongly recommend that you reconfigure the utility to secure your system.Use the DeskLock tool to:
- Choose settings so that an operator usingFactoryTalk Viewcannot gain access to functionality not expressly configured by the system integrator.
- Hide items on the Windows Explorer desktop, including theTaskbarandStartmenu.
- Disable key combinations that are used to perform specific Windows actions such as accessing theTask Manager.TIP:In the DeskLock utility, all Windows hot keys are disabled except theWindows Logo + Lcombination, which still locks the Windows Desktop.
- Provide access to the Microsoft Management Console for more advanced configuration.
Provide Feedback