Create a DeskLock HotKeyDisable button
Use the
Insert an ActiveX Control
dialog box to create a DeskLock HotKeyDisable
button.To create a DeskLock HotKeyDisable button
- From theObjectsmenu, selectActiveX Control.
- Drag the ActiveX tool to draw a rectangle the size you want the object to be.
- In theInsert an ActiveX Controldialog box, selectDeskLock HotKeyDisable Buttonfrom the list of registered objects.
- Double-click the button to open itsPropertiesdialog box.
- In thePropertiesdialog box, specify how the button looks, the action to be initiated by the button, and its tags or expressions.
Provide Feedback