Set up connections for the DeskLock HotKeyDisable button (Connections tab)

Use the
Connections
tab to set up tags and expressions for the
DeskLock HotKeyDisable
button.
To set up tags and expressions for the DeskLock HotKeyDisable button
  1. In the
    Graphics Display
    editor, double-click the button to open its
    Properties
    dialog box.
  2. Click the
    Connections
    tab.
  3. Assign a tag or expression to these connections:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal