Set up the hot keys to disable (General tab)
The
DeskLock HotKeyDisable
button allows you to specify what hot key sequences will be disabled when the button is pressed.To select the hot key sequence to be disabled by the button
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click theGeneraltab.
- From theHot Keylist, select the hot key sequence to be disabled when the button is pressed.
Provide Feedback