DeskLock HotKeyDisable button General tab options
The following table shows the options on the
General
tab in the DeskLock HotKeyDisable Button Properties
dialog box.Options | Descriptions |
|---|---|
Hot key settings | From the list, select the hot key sequence to be disabled when the button is pressed. |
Hot key | |
Task Switch | Specifies the Alt+Tab , Ctrl+Esc , and Alt+Esc key sequences for task switching |
Task Manager | Specifies the Ctrl+Shift+Esc key sequence for task switching |
WinKeys | Specifies the special Window key sequences on the keyboard |
Provide Feedback