Set up how the DeskLock HotKeyDisable button looks (Appearance tab)
The
DeskLock HotKeyDisable
button can be set up to change its caption color and image (if any) depending on whether the assigned hot key combination is enabled or disabled.To set up the appearance options for the DeskLock HotKeyDisable button
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click theAppearancetab.
- Specify these properties:
- Caption text, font size and style
- Caption text color and background color for disabled and enabled states
- Image displayed for disabled and enabled states (if any)
Provide Feedback