DeskLock HotKeyDisable button Appearance tab options
The following table shows the options on the
Appearance
tab in the DeskLock HotKeyDisable Button Properties
dialog box.Options | Descriptions |
|---|---|
Caption | In the text box, specify the text for the button. By default, the button's caption is DeskLockHotKeyDisableButton1 . The text appears on the face of the button, and changes color when the button is pressed to enable or disable the hot key sequence specified in the General tab. |
Font | Select the font to use for the caption. |
Size | Select the font size to use for the caption. |
Bold, Italic, Underline | Select a font style for the caption, if required. |
Hot key disabled color | This box shows the current color for the caption when the hot key sequence is disabled. Click it to select another color. |
Hot key enabled color | This box shows the current color for the caption when the hot key sequence is enabled. Click it to select another color. |
Background color setting | |
Hot key disabled color | This box shows the current background color for the caption when the hot key sequence is disabled. Click it to select another color. |
Hot key enabled color | This box shows the current background color for the caption when the hot key sequence is enabled. Click it to select another color. |
Image setting | |
Hot key disabled image | Click the Browse button to open a standard search window. Navigate to the desired image and click Open . The image appears on the face of the button when the hot key sequence specified in the General tab is disabled.To remove the image from the button, click Clear . |
Hot key enabled image | Click the Browse button to open a standard search window. Navigate to the desired image and click Open . The image appears on the face of the button when the hot key sequence specified in the General tab is enabled.To remove the image from the button, click Clear . |
Provide Feedback