DeskLock HotKeyDisable button Connections tab options
The following table shows the options on the
Connections
tab in the DeskLock HotKeyDisable Button Properties
dialog box.Options | Descriptions |
|---|---|
Enable | A read connection. Assign a tag or an expression to this connection. The application reads the value of the connection at the data source, and updates the object’s display to reflect the state corresponding to the value. If you assign an expression, the application calculates the value of the expression and updates the object’s display to reflect the state corresponding to the value. |
Visible | A read connection. Assign a tag or an expression to this connection. The application reads the value of the connection at the data source, and updates the object’s display to reflect the state corresponding to the value. If you assign an expression, the application calculates the value of the expression and updates the object’s display to reflect the state corresponding to the value. |
Name | This column shows the name of the connection. |
Value update direction | This column shows an arrow to indicate which way data can flow between the connection and the data source. ¬ data source updates the connection (read connection) |
Tag/Expression | Type the tag name or expression associated with the connection. If a tag or expression has already been selected, it is displayed here. |
Tag button (...) | Click this button to open the Tag Browser dialog box, and choose a tag instead of typing the tag name in the Tag/Expression column. |
Exprn button (...) | Click this button to open the Expression editor, and create an expression instead of typing the expression in the Tag/Expression column. |
Provide Feedback