Set up DeskLock
Use DeskLock to replace the standard Windows desktop with a customized one intended to prevent operators from having access to operating system functions, like restarting Windows or shutting down tasks.
IMPORTANT:
Be sure to leave a way for the Windows administrator to access DeskLock setup, or there could be no future access to it at all.
To set up DeskLock
- Log on to Windows as a user with administrator rights.
- From WindowsStartmenu, selectAll apps>Rockwell Software>DeskLock.
- In theDeskLockdialog box, clickSet Up DeskLock.
- On theLogontab, set up logon.
- On theDesktoptab, specify how your desktop will look at runtime - whether to use a Windows desktop or DeskLock.
- On thePasswordtab, specify which DeskLock actions require a password, and what the DeskLock password will be.
- On theBehaviortab, specify what buttons will be available in theWindows Securitydialog box that opens when the key combinationCtrl+Alt+Delis pressed, and what other key combinations will be enabled or disabled when DeskLock is running.
- ClickOKto save the changes, and then restart your system.
- To return to the Windows defaults for all the settings changed during DeskLock setup, clickDefaults.TIP:No matter which tabDefaultbutton is pressed, all the changes made in all the tabs will be reset to the Windows defaults. Changes made in the Microsoft Management Console will not be reset. These must be reset individually in the Microsoft Management Console.
Provide Feedback