Set up password

In the
Password
tab, specify which DeskLock actions require a password. A single password, which you can change in this tab, is used for all actions.
To return to the Windows defaults for all the settings changed during DeskLock setup, click the
Defaults
button. This does not reset changes made in the Microsoft Management Console.
The password specified here is for DeskLock only. To set up a password for automatic logon for Windows , use the Logon tab.
To set up the password for DeskLock
  1. Select the actions for which you require passwords.
  2. Click the
    Change Password
    button to open a dialog box to change the password for these tasks.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal