Password setup options
The following table shows the options on the
Password
tab in the DeskLock Setup
dialog box.Options | Descriptions |
|---|---|
Require password to restart Windows from DeskLock | Select this option to require a password when restarting Windows from DeskLock. |
Require password to exit DeskLock | Select this option to require a password when exiting from DeskLock. |
Require password to open this dialog box again | Select this option to require a password to open the DeskLock Setup dialog box.If you require passwords for all these functions, be sure the Windows administrator is aware of the passwords, otherwise there could be no access to this dialog box in future. |
Provide Feedback