Set up DeskLock behavior
Use the check boxes in the
Behavior
tab to specify how DeskLock behaves when active.To set up DeskLock behavior
- In theCtrl+Alt+Del Window Optionsframe, select or clear the boxes that disable buttons in theWindows Securitydialog box that appears when the key combinationCtrl+Alt+Delis pressed. The buttons will still be visible, but will not be active.
- If you need to make other changes to Microsoft Windows Local Group Policy settings, open the Microsoft Management Console and make those changes.
- In theHot Key settingsframe, select eor clear the boxes that disable the key combinations that function as a normal part of Windows. If any of these boxes are selected, you can also specify a time period of inactivity. If no keyboard or mouse activity is detected for the specified period, the key combinations whose boxes are selected will automatically be disabled.TIP:DeskLock installation also provides two control buttons that can be placed on a FactoryTalk View SE graphic display: aDeskLock HotKeyDisablebutton that can be used to disable the hot key combinations, and a SysRestart button that can shut down and restart the operating system.If theDeskLock setupdialog box is opened, or if DeskLock exits, the hot key combinations will be enabled.
Provide Feedback