DeskLock behavior setup options
The following table shows the options on the
Behavior
tab in the DeskLock Setup
dialog box.Options | Descriptions |
|---|---|
Ctrl+Alt+Del Window Options | The check boxes in this frame are linked to the Microsoft Windows Local Group policy settings. These settings can also be changed in the Microsoft Management Console. When the Behavior tab is first opened, whether the check boxes are selected, or not reflects the existing settings in the Microsoft Management Console. When the OK button is pressed, changes made in this tab may override runtime settings in the Management Console made through other means. |
Disable Shutdown Windows | Select this check box to disable the Shutdown Windows button on the Windows Security dialog box and prevent users from shutting down or restarting Windows.This option is linked to the Local Group policy setting Remove and prevent access to the Shut Down Command , located in the Administrative Templates\Start Menu and Taskbar folder of the Microsoft Management Console. |
Disable Task Manager | Select this check box to disable the Task Manager button on the Windows Security dialog box and prevent users from accessing the Task Manager.This option is linked to the Local Group policy setting Remove Task Manager , located in the Administrative Templates\System\Ctrl+Alt+Del Options folder of the Microsoft Management Console. |
Disable Lock Computer | Select this check box to disable the Task Manager button on the Windows Security dialog box and prevent users from accessing the Task Manager.This option is linked to the Local Group policy setting Remove Lock Computer , located in the Administrative Templates\System\Ctrl+Alt+Del Options folder of the Microsoft Management Console. |
Disable Change Password | Select this check box to disable the Task Manager button on the Windows Security dialog box and prevent users from accessing the Task Manager.This option is linked to the Local Group policy setting Remove Change Password , located in the Administrative Templates\System\Ctrl+Alt+Del Options folder of the Microsoft Management Console. |
Disable Logoff | Select this check box to disable the Task Manager button on the Windows Security dialog box and prevent users from accessing the Task Manager.This option is linked to the Local Group policy setting Remove Logoff , located in the Administrative Templates\System\Ctrl+Alt+Del Options folder of the Microsoft Management Console. |
Open the Microsoft Management Console for Local Group Policies | The console opens by default to the Console Root\Local Computer Policy\User Configuration\Administrative Templates\System\Ctrl+Alt+Del Options folder. |
Hot Key Settings | The check boxes in this frame disable the specified key combinations while DeskLock is running. If DeskLock is closed, or if the DeskLock Setup dialog box is opened, the key combinations will be enabled.These settings can also be changed through the HotKey control button in graphic displays, or through VBA code. When the Behavior tab is first opened, the state of the check boxes reflects the existing settings. If a check box is cleared, both the last setting in DeskLock and the current runtime setting are set to enabled. If a check box is selected, both the last Desklock setting and the current runtime setting are set to disabled. If a check box appears grayed and selected, the last DeskLock setting was enabled, but that key combination has been disabled from outside this tab, probably through a control button. Click a grayed box once to select the check box, and twice to clear it.When the OK button is pressed, if a checkbox is selected, or grayed and selected, the key combination will be disabled. If the check box is cleared, the key combination will remain in effect. |
Disable Task Switch keys (Alt+Tab, Ctrl+Esc, Alt+Esc) | Select this check box to disable the task key combinations. This prevents users from showing and selecting the running applications ( Alt+Tab ), switching between the applications on the task bar (Ctrl+Esc ), and showing the Start menu (Alt+Esc ). |
Disable Task Manager keys (Ctrl+Shift+Esc) | Select this check box to disable the Ctrl+Shift+Esc key combination and prevent users from opening the Task Manager dialog box. |
Disable Windows hot keys (Windows Logo+?) | Select this check box to disable any hot key combinations that use the Windows logo ( ) key. |
Automatically disable selected hot keys after a period of inactivity | If any of the above check boxes are selected, this check box becomes available. Select this check box to activate the list of time options. |
Seconds | Select a time period in seconds from the list. If no keyboard, or mouse activity is detected for the specified number of seconds, the key combinations whose boxes are selected will be automatically disabled. This prevents any of the DeskLock settings being indefinitely overridden by a runtime setting. Options are 15 , 20 , 25 , 30 , 45 , 60 , 90 , and 120 . |
Defaults | To return to the Windows defaults for all the settings changed during DeskLock setup, click this button. This does not reset changes made in the Microsoft Management Console. |
Provide Feedback
) key.