Set up desktop

In the
Desktop
tab, specify how your desktop look and behave at runtime.
To set up the desktop
  1. Specify which desktop is to be used the next time Windows starts.
    When you select
    Replace existing desktop with DeskLock
    , the
    DeskLock Applications Programs
    options appear.
  2. For each program that is to run when DeskLock starts, or is to have a button on the desktop, fill in the information requested in the
    Programs
    part of the tab.
    TIP:
    To return to the Windows defaults for all the settings changed during DeskLock setup, click the
    Defaults
    button. This does not reset changes made in the Microsoft Management Console.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal