What is a trend?

A trend monitors and shows real-time and historical data. You can graph data as a time plot or as an x/y plot, where two or more sets of values are plotted to show the relationship between them.
Use a trend to:
  • Show data as it is read from the data source.
  • View changes in data over time.
  • Show isolated or non-isolated graphs.
  • Plot one variable against one or more others in XY plots.
  • Print data.
Use these button objects with trends:
A pen on the runtime trend chart represents data from the tag or expression that you assign to the pen on the
Connections
tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal