Set up the vertical axis for the trend

Use the
Vertical
tab of the
Trend Object Properties
dialog box to specify the range of values to show on the vertical axis.
To set up the vertical axis
  1. In the
    Graphics Display
    editor, double-click the trend to open the
    Trend Object Properties
    dialog box.
  2. Click the
    Y-Axis
    tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal