Set up the horizontal axis for the trend
Use the
X-Axis
tab of the Trend Object Properties
dialog box to specify the horizontal axis for the trend. The horizontal axis represents time, for a standard line chart, or the selected pen value, for an XY plot.
TIP:
Select the chart style on the
General
tab.To set up the horizontal axis
- In theGraphics Displayeditor, double-click the trend to open theTrend Object Propertiesdialog box.
- Click theX-Axistab.
Provide Feedback