Set up how the trend works at runtime
Use the
Display
tab of the Trend Object Properties
dialog box to specify how the trend works at runtime.To set up how the trend works at runtime
- In theGraphics Displayeditor, double-click the trend to open theTrend Object Propertiesdialog box.
- Click theDisplaytab.
- How the trend looks
- Whether the trend scrolls at runtime
- How much extra data to store in the bufferTIP:Changing the background color does not change the chart window area. The window color and style can be changed in the Property Panel.
Provide Feedback