Set up pens for the trend
Use the
Pens
tab of the Trend Object Properties
dialog box to specify pens for the trend.Prerequisite
- Assign tags or expressions to the pens on theConnectionstab.
To set up pens
- In theGraphics Displayeditor, double-click the trend to open theTrend Object Propertiesdialog box.
- Click thePenstab.
- TIP:Tag names will show after tags are assigned on theConnectionstab.
Provide Feedback