Apply attributes to multiple pens
You can apply attributes to multiple pens on the
Pens
tab of the Trend Object Properties
dialog box.To apply attributes to multiple pens
- In theGraphics Displayeditor, double-click the trend to open theTrend Object Propertiesdialog box.
- Click thePenstab.
- Select multiple pens in thePen Attributesbox by pressing and holding theCtrlkey while clicking the tag names.
- In theMultiple Pen Editsspreadsheet, specify the attributes you want to apply to all of the selected pens, and then clickApply to Selected Pens.
Provide Feedback