About the Status Bar
The Status Bar at the bottom of the FactoryTalk AssetCentre window shows:
- the status of the database usage (only shows if the database limitations is enabled in theOptions: Database Limitationsdialog box)
- the currently logged on FactoryTalk user
- the status of the connection to the server
- the number of connected agent computers in the system
Select
View > Status Bar
to hide or show the Status Bar.Provide Feedback