Command Editor - Compare dialog box

How do I open the Command Editor - Compare dialog box?
  1. Select
    Tools > Options
    .
  2. In the
    Options
    dialog box, under
    Category
    on the left, select
    Custom Devices
    .
  3. In the
    Compare Configuration
    section of the right pane, click browse_button_small besides the blank field of
    Command
    .
Use the
Command Editor - Compare
dialog box to view and edit the compare configuration command of custom devices.
The
Command Editor - Compare
dialog box includes the following items:
  • Program
    Specifies the available application files to run compare operations for custom devices.
    FactoryTalk AssetCentre supports the following types of application files: *.exe, *.bat, *.vbs, and *.ps1.
  • Arguments
    The left combo box lists the available arguments to compose a command line for the compare operations. The right combo box lists the arguments that are selected to compose the command line for the compare operations.
    To select an available argument to compose the command line, click the argument in the left combo box, and then click right arrow. The selected argument will be added to the right combo box. You can add one or more available arguments from the left combo box to the right combo box. For the arguments in the right combo box, you can use left arrow to move an argument back to the left combo box, or use up arrow and down arrow to change their sequences.
  • Command Preview
    Shows the preview of the final command line with the specified program and arguments.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal