Command Editor - Post Backup dialog box
How do I open the Command Editor - Post Backup dialog box?
- SelectTools > Options.
- In theOptionsdialog box, underCategoryon the left, selectCustom Devices.
- In thePostBackup Configurationsection of the right pane, click
besides the blank field of Command.
Use the
Command Editor - Post Backup
dialog box to view and edit the post-backup configuration of custom devices.The
Command Editor - Post Backup
dialog box includes the following items:- ProgramSpecifies the available application files to perform the post-backup operations for custom devices.FactoryTalk AssetCentre supports the following types of application files: *.exe, *.bat, *.vbs, and *.ps1.
- ArgumentsThe left combo box lists the available arguments to compose a command line for the post backup operations. The right combo box lists the arguments that are selected to compose the command line for the post backup operations.To select an available argument to compose the command line, click the argument in the left combo box, and then click
. The selected argument will be added to the right combo box. You can add one or more available arguments from the left combo box to the right combo box. For the arguments in the right combo box, you can use
to move an argument back to the left combo box, or use
and
to change their sequences. - Command PreviewShows the preview of the final command line with the specified program and arguments.
Provide Feedback