Make sure IIS is running on the server

To properly run FactoryTalk AssetCentre, you need to make sure IIS is running on the server computer.
To make sure IIS is running on the server computer
  1. From Windows
    Start
    menu, Right-click
    Computer
    , and select
    Manage
    . This starts the Computer Management console.
  2. In the Computer Management console, open
    Services and Applications
    .
  3. Click
    Internet Information Services
    . The right pane lists the Internet services running under IIS. Open the
    Web Sites
    folder, and make sure the web site used for FactoryTalk AssetCentre (generally the Default Web Site) is Running. If it is not, continue to the next step. If more than one web site is listed here, ask your system administrator. The web site for FactoryTalk AssetCentre was specified during the IIS portion of the FactoryTalk AssetCentre Server installation.
  4. To start the service, right-click on the icon for the web site used for FactoryTalk AssetCentre (in most cases
    Default Web Sites
    ) and select
    Start
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal