Tab is blank or says reading information
If the
Design
button is unavailable and the Schedules
, Searches
, and Archive
tabs in the Workspace Pane all are blank or show the message reading information
for an inordinately long time, reboot the client computer.You might also check to make sure IIS is running on the server computer.
Provide Feedback