Schneider Controller (Control Expert) operation properties for disaster recovery
Following are all possible settings for disaster recovery schedules for Schneider Controller
(Control Expert) assets.
These settings are used for two purposes:
- Specify default disaster recovery schedule settings for Schneider Controller (Control Expert) inTools>Options.
- Specify the settings of a particular Schneider Controller (Control Expert) asset in an existing schedule in theSchedulestab. Changes to the settings within a schedule override the default settings for that instance.
Unless noted otherwise, each setting applies to backup schedules and backup and compare schedules.
IMPORTANT:
- Make sure that the FactoryTalk AssetCentre Agent Controller is running as an application. For more information, see FactoryTalk AssetCentre Agent Controller Launch Control Panel.
- For Schneider Control Expert using Unity DIF 8.0 to compare projects, FIPS must be disabled for communication to work properly.
(Backup and compare schedules only) Event Settings
- Backup Compare Partner(Only available when editing an existing schedule, not when setting defaults.) Specify the version of the backup data file to compare to the Schneider Controller (Control Expert) asset files.
- Create New Backup VersionSet toAlwaysto create a backup version even if it is the same as the last compared backup version. This is the default setting.Set toOn Differences Foundto create a backup version only if differences are found. If the existing backup is the same as the information in the controller aside from excluded data blocks, then no backup is saved.
Asset specific properties
- (Backup and compare schedules only) Create New Backup Version Due to Unmatched PasswordsIf the archive version and the new backup file have different encryption passwords, they cannot be compared.When the new backup file has a different encryption password:
- Set toTrueto create a backup version for it.
- Set toFalseto not create a backup version for it.
- Only Report DifferencesSet toTrueto generate a report that only shows differences when differences are found and the task is completed successfully.
Email notification
You can type email recipients' addresses separated by semicolons (;) or select addresses from the FactoryTalk AssetCentre Address Book. To select addresses from the Address Book, click in the field, and then click
. Complete the
. Complete the Contacts and Groups
dialog box.An email message will be sent to only one of these lists. For example, if differences are found when a backup and compare schedule runs, an email is sent to those on the
Event Compare Differences Detected
list. No email is sent to those on the Event Completed
list.- (Backup and compare schedules only) Event Compare Differences DetectedThe email addresses separated by semicolons (;) to which the notification will be sent if the compare finds differences between the specified backup data or configuration data version and the data on the physical device.
- Event CompletedThe email addresses separated by semicolons (;) to which notification will be sent when the operation completes for the asset. If a backup and compare schedule completes without differences, an email is sent to this list. If it completes with differences, an email is sent to theEvent Compare Differences Detectedlist, not this list.
- Event FailedThe email addresses separated by semicolons (;) to which notification will be sent when the operation fails.
(Backup and compare schedules only) Attach report to email
- Event Completed Differences DetectedThis defaults toTrueto attach a report of differences to the email if the backup and compare schedule finds differences between the specified backup data version and the data on the physical device. SelectFalseto send an email without an attached report.
Provide Feedback