Delete a schedule
Delete schedules that you no longer want to view or run. You must stop a running schedule and make the schedule inactive before you can delete it. When you delete a schedule, it is removed from the
Schedules
tab and the FactoryTalk AssetCentre database.Prerequisites
- To delete schedules, you must haveDelete a schedulepermission.
To delete a schedule
- SelectView > Schedules, or click theSchedulesbutton.
- If the schedule is running, stop the schedule before deleting it.
- If the schedule is active, deactivate the schedule before deleting it. In the schedule row, clear theActivecheck box.
- Select the schedule to delete. To select multiple schedules, useCtrl-ClickorShift-Click.
- PressDeleteor click
. - When prompted to delete the schedule, clickYes.
Provide Feedback