Run a schedule immediately
Run a schedule immediately without waiting for its next scheduled run time. You can manually run schedules with Waiting to Run status. This does not affect the active schedule's start time. You cannot manually run a schedule that has Running status. A schedule that is executing as a Run Now event cannot be activated.
Prerequisites
- To run schedules, you must haveCommand a schedulepermission.
- To activate schedules, you must haveEdit a scheduleandCommand a schedulepermission.
To run a schedule immediately
- SelectView > Schedules, or click theSchedulesbutton.
- Select the schedule to run. You cannot run a schedule if the schedule's status is Running.
- Click theRun Nowbutton.TIP:You can also right-click the schedule row and selectRun Now.
Provide Feedback