Run a schedule automatically
Activate a schedule so that it runs at its next scheduled time.
Prerequisites
- To run schedules, you must haveCommand a schedulepermission.
- To activate schedules, you must haveEdit a scheduleandCommand a schedulepermission.
To run a schedule automatically
- SelectView > Schedules, or click theSchedulesbutton.
- Next to the schedule you want to activate, select theActivecheck box.If the selected schedule is to run daily at 4:00 P.M., the schedule will run next at 4:00 P.M. today (or 4:00 P.M. tomorrow if it is later than 4:00 P.M. today).
Provide Feedback