Export compare engine configurations

Comparison software configurations (the location of the software, command line parameters, file types for which to use the comparison software) can be exported to a file, which can be imported to another FactoryTalk AssetCentre server.
To export compare engine configurations
  1. Select
    Tools > Options
    .
  2. In the left column, click
    Compare Engines
    .
  3. In the right pane, click Export_button to export.
  4. Use the
    Select Compare Engine
    dialog box to specify which compare engines to export. You can use
    Shift-Click
    and
    Ctrl-Click
    to select multiple compare engines. Click
    OK
    .
  5. Use the
    Save As
    dialog box to provide a filename and location for the exported list.
  6. Transfer the saved file to the FactoryTalk AssetCentre server on which you want to import the settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal