Impact on schedules and agent groups after moving an asset

Moving an asset brings impacts on schedules and agent groups.
Impact on schedules
  • If the asset is the starting point (top-level asset) in a schedule, then that schedule will not change. That schedule will still be associated with the asset.
  • If the container from which you moved the asset has a schedule associated with it, the asset is removed from that schedule.
  • If the container into which you moved the asset has a schedule associated with it, the asset is added to that schedule, but with the default settings determined by the
    Options
    dialog box.
Impact on agent groups
  • If the asset inherits agent group from its parent, its Agent Group property will be updated as the target parent’s agent group.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal