Impact on schedules after copying an asset
If the asset had its own schedule, then that schedule will not change. That schedule will be associated with the original instance of the asset. The schedule will not be copied to the new instance of the asset. If you rename the original asset, that will be reflected in the schedule. If you rename the new instance of the asset, that will NOT be reflected in the schedule because the schedule is not associated with the new instance of the asset.
If the container from which the asset was copied has a schedule associated with it, that schedule remains unchanged.
If the container into which the asset is copied has a schedule associated with it, the asset is added to that schedule, but with the default settings determined by the
Options
dialog box.Provide Feedback