Link Properties dialog box
How do I open the Link Properties dialog box?
- Enter Design mode then right-click a device in the tree and selectProperties. (If you are not in Design mode, and you haveReadpermission, you can view but not edit the properties.)
- Keyboard shortcut: Select the link and pressF4.
Use the
Link Properties
dialog box to view or change the settings for a link.Provide Feedback