Items in Link Properties dialog box

Items in the dialog box include:
  • Link target
    To link to another file or binder, navigate the asset tree shown here to select the file or binder.
  • Link Name
    To change the name of the link in the Asset View, edit this field.
  • Description
    (Optional) Enter a description of the link. The description will appear on the
    Archive
    tab when the link is selected in the Asset View.
  • red_circle_exclamation
    If you see this icon next to any of the fields above, it means the current information in that field is not valid. Hover the pointer over the icon to show a message indicating what is required.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal