FTP Address dialog box

How do I open the FTP Address dialog box?
You can open the
FTP Address
dialog box while adding the ABB Robot, FANUC Robot, Motoman Robot, or Generic FTP Device asset to the asset tree or while editing its properties.
While adding the asset to the asset tree:
  1. If you are not already in Design mode, click design_mode_button.
  2. Drag an ABB Robot, FANUC Robot, Motoman Robot, or Generic FTP Device asset from the Asset Catalog to a container in the Asset View.
  3. Click anywhere within the
    Addressing Info
    field and click browse_button_small.
While editing the asset's properties:
  1. If you are not already in Design mode, click design_mode_button.
  2. Double-click an ABB Robot, FANUC Robot, Motoman Robot, or Generic FTP Device asset in the tree.
  3. Click anywhere within the
    Addressing Info
    field and click browse_button_small.
Use the
FTP Address
dialog box to specify addressing information for the ABB Robot, FANUC Robot, Motoman Robot, or Generic FTP Device asset.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal