Add ABB Robot dialog box
How do I open the Add ABB Robot dialog box?
- To enter Design mode if you are not already in it, select
. - In the Asset Catalog, expand theLegacy Device Itemsnode.
- Drag an ABB Robot asset onto the tree in the Asset View.
Use the
Add ABB Robot
dialog box to add an ABB robot to the asset tree. You can add an ABB robot in the root or in a container.The device is added to the asset tree as soon as this dialog box opens. Clicking
Cancel
in this dialog box abandons any changes made to the device properties, but leaves the device in the tree.Provide Feedback