Add FANUC Robot dialog box

How do I open the Add FANUC Robot dialog box?
  1. To enter Design mode if you are not already in it, click design_mode_button.
  2. In the Asset Catalog, expand the
    Legacy Device Items
    node.
  3. Drag a FANUC Robot asset onto the tree in the Asset View.
Use the
Add FANUC Robot
dialog box to add a FANUC robot to the asset tree. You can add a FANUC robot in the root or in a container.
The device is added to the asset tree as soon as this dialog box opens. Clicking
Cancel
in this dialog box abandons any changes made to the device properties, but leaves the device in the tree.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal