Add Link dialog box
How do I open the Add Link dialog box?
- To enter Design mode if you are not already in it, click
. - In the Asset Catalog, expand theFile and Folder Itemsnode.
- Drag a Link asset onto the tree in the Asset View.
Use the
Add Link
dialog box to place a link in the asset tree to a file or binder asset that is already included in a different location in the tree. You can place a Link anywhere in the tree.Provide Feedback