Items in Add Link dialog box
Items in the dialog box include:
- Link targetNavigate the asset tree displayed here to find the file or binder to which you want to add a link. Click the file or binder to select it.
- Link NameOnce you've selected a file or binder in theLink targetfield, this field is automatically filled in. If you want to change the name of the link in the Asset View, edit this field.
- Description(Optional) Enter a description of the link. The description will appear on theArchivetab when the link is selected in the Asset View. The description can be a maximum of 260 characters.
If you see this icon next to any of the fields above, it means the current information in that field is not valid. Hover the pointer over the icon to show a message indicating what is required.
Provide Feedback