Add Folder dialog box
How do I open the Add Folder dialog box?
You can open the
Add Folder
dialog box either while adding a folder to the asset tree or while specifying the configuration files for a robot.While adding a folder to the asset tree:
- To enter Design mode if you are not already in it, click
. - In the Asset catalog, expand theFile and Folder Itemsnode.
- Drag a folder to a container or device in the Asset View.
While adding files to a robot:
- To enter Design mode if you are not already in it, click
. - Drag a robot device from the Asset Catalog to the tree or right-click a robot in the tree and selectProperties.
- Click anywhere within theConfiguration Datafield and then click
. - In theConfiguration Data Browserdialog box, clickAdd.
Use the
Add Folder
dialog box to add a folder to the asset tree. You can place a folder anywhere in the tree.Provide Feedback