Items in Add Folder dialog box

Items in the dialog box:
  • Folder
    The path and name of the folder you want to add. You can type the path directly in this field, but it is best to use the Browse button to avoid typographical or syntax errors.
  • Browse
    Opens a dialog box in which you can navigate your computer's hard drive or other locations to select the folder you want to add to the asset tree.
  • Add all this folder's contents as well
    Check this box to add all the files within the folder. Otherwise only an empty folder will be added to the asset tree.
  • Description
    (Optional) Type a brief description of the folder. This description will be displayed in the
    Archive
    tab when the folder is selected. The description can be a maximum of 260 characters.
  • Comments
    (Optional) Type a comment about this action (adding the folder). This comment will appear in the
    History
    tab in
    Archive
    and the Audit log record for this action.
  • red_circle_exclamation
    If you see this icon next to any of the fields above, it means the current information in that field is not valid. Hover the pointer over the icon to display a message indicating what is required.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal