Add Files dialog box
How do I open the Add Files dialog box?
- To enter Design mode if you are not already in it, click
. - In the Asset catalog, expand theFile and Folder Itemsnode.
- Drag a file to a container or device in the Asset View.
Use the
Add Files
dialog box to add files to the asset tree.Provide Feedback