Add files to the asset tree
You can use the
Add Files
dialog box to add files to the asset tree.To add files:
- ClickAdd Files.
- Navigate to the directory containing the file or files you want to add.
- Select the file and clickOpen. Use Ctrl-click and Shift-click to select multiple files.
- Verify in the list of files that the correct files were selected. If you need to remove any files, select them in the list and clickRemove.
- (Optional) In theDescriptionfield, type a brief description of the files, such asMy Processor program and documentation files. This description will be shown in theArchivetab when the file is selected. The description can be a maximum of 260 characters.
- (Optional) In theCommentsfield, type a comment about this action (adding the files). The comment for this action will appear in theHistorytab inArchiveand the Audit log record for this action.
Provide Feedback