Items in Add Asset Inventory dialog box
Items in the dialog box include:
- (Parent)(Read-only) This field shows the name of the container into which the Asset Inventory asset is being added.
- Description(Optional) Type a description for the Asset Inventory asset. The description shows in theArchivetab when the Asset Inventory asset is selected. The description can be a maximum of 260 characters.
- NameEnter a unique and meaningful name for the asset. This name shows in the asset tree. The software defaults toAsset Inventory. The name must be unique within the parent container. That is, you can have two assets with the same name in the asset tree, they just can't be in the same container. If you add an asset into a container that has an asset of the same name, FactoryTalk AssetCentre appends a number (like_2) to the asset name to ensure uniqueness.Asset names can be a maximum of 260 characters. The characters \ / : * ? " < > | are not allowed. The character pair &# is not allowed. A space, tab, underscore (_) or dollar sign ($) cannot be the first character in a name, but can be used elsewhere in the name. The following Microsoft Windows device names cannot be used as asset names, whether upper or lower case, with or without the colon: CON:, PRN:, AUX:, NUL:, COM1:, COM2:, COM3:, COM4:, COM5:, COM6:, COM7:, COM8:, COM9:, LPT1:, LPT2:, LPT3:, LPT4:, LPT5:, LPT6:, LPT7:, LPT8:, and LPT9. For example,Auxiliary Linewould be a valid name whereasAux Linewould not.
- Backup DataSpecify the backup file to use for Backup or Backup and Compare operations. FactoryTalk AssetCentre uses a .raai file as the backup file for Asset Inventory. To specify a backup file, click in this field and then click
. The Backup Data Browserdialog box opens.In most cases, when configuring an Asset Inventory asset for the first time, the backup file does not exist yet. In this situation you can choose to leave Backup Data unspecified or manually specify a backup file.If you do not specify a backup file, one is automatically created the first time a backup schedule runs for this asset. The file is a .raai file, which stores the scanning result after Asset Inventory backup or backup and compare schedule completes. The file name isAssetName_Backup, whereAssetNameis the name of the Asset Inventory asset as given in theNamefield in this dialog box. The new backup file is placed under Asset Inventory in the asset tree. The schedule is also updated to use the new file.If you want to specify a backup file, select a specific .raai file on your computer or on a network location, and then add it as the backup file for Asset Inventory. - Scanning ConfigurationClick in this field and then click
to configure the scanning properties for Asset Inventory. In the Scanning Configurationdialog box, configure the following scanning modes:- Scan devices using CIP
- Scan devices using SNMP
- Scan software using WMIClickAdvanced Settingsto configure more settings.
- Agent GroupClick in this field and then click
to select the agent group for Asset Inventory.- When adding Asset Inventory under the root, the default value of Agent Group isSystem Default.
- When adding Asset Inventory under a container, the default value of Agent Group isInherit from parent: the parent container’s Agent Group property.
- Properties Configuration(Optional) This box shows the number of default extended properties configured by theOptions dialog box: Extended Properties. To configure extended properties for the asset, click in this box, and then click
. In the Extended Propertiesdialog box, edit, add, or delete extended properties.
Provide Feedback