Add Asset Inventory dialog box

How do I open the Add Asset Inventory dialog box?
  1. If you are not in Design mode, click design_mode_button.
  2. In the Asset Catalog, expand the
    Asset Inventory Items
    node.
  3. Drag an Asset Inventory asset onto the tree in the Asset View.
Use the
Add Asset Inventory
dialog box to add an Asset Inventory asset to the asset tree. You can add an Asset Inventory in the root or in a container.
The Asset Inventory asset is added to the asset tree as soon as this dialog box opens. Clicking
Cancel
in this dialog box abandons any changes made to the asset properties, but leaves the asset in the tree.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal