Advanced Settings dialog box
How do I open the Advanced Settings dialog box?
You can open the
Advanced Settings
dialog box while adding an Asset Inventory asset to the asset tree or editing the asset's properties.While adding an Asset Inventory asset to the asset tree:
- If you are not in Design mode, click
. - Drag Asset Inventory from the Asset Catalog to a container in the Asset View.
- Click anywhere within theScanning Configurationfield and then click
. - In theScanning Configurationdialog box, clickAdvanced Settings.
While editing an Asset Inventory asset's properties:
- If you are not in Design mode, click
. - Double-click Asset Inventory in the tree.
- Click anywhere within theScanning Configurationfield and then click
. - In theScanning Configurationdialog box, clickAdvanced Settings.
User the
Advanced Settings
dialog box to configure the advanced settings for the scanning properties.Provide Feedback