Items in Scanning Configuration dialog box
Items in the dialog box include:
- Scan devices using CIPIMPORTANT:When performing a CIP scan with an Ethernet/IP, predicting the depth level of discoverable bridged assets can be difficult. Given that the CIP imposes a depth limitation of seven levels, we recommend creating additional Asset Inventory disaster recovery schedules to ensure the capture of more devices if you are using an Ethernet/IP to perform a CIP scan. While it is possible to exceed seven levels when bridging to different networks using DeviceNet or ControlNet, the actual depth level depends on the specific network structure.
- Start scanning from this deviceClick
next to the Start scanning from this devicefield and select the device to start scanning. - Maximum scanning depthEnter the value for maximum scanning depth. The valid value is between 1 and 100. You need to clear theUnlimited scanningcheck box before entering the value.
- Unlimited scanningKeep theUnlimited scanningcheck box selected if you don't want to limit the scanning depth. Clear the check box to enter the maximum scanning depth.
- Scan devices using SNMP
- If theIP address rangeoption is selected, specify theStart IP addressandEnd IP address.Keep theUnlimited hopscheck box selected if you don't want to limit the number of hops. Clear the check box to enter the maximum number of hops.
- If theIP subnetoption is selected, specify theNetwork IP address,Subnet mask, andHost address range.
- Scan software using WMITIP:Before performing an Asset Inventory WMI scan on a remote computer, please ensure:
- Port 135 on the remote computer is turned on.
- The Remote Procedure Call (RPC) service is running.
- Firewall on the remote computer is set to allow any IP Address or Specified IP that the Scan server used.To configure the Windows Defender Firewall1. Go toControl Panel > System Security > Windows Defender Firewall.2. On the left column, selectAllow an app or feature through Windows Defender Firewall, and then select theWindows Management Instrumentation (WMI)check box. For some operating systems, you may have to skip to step 3 and step 4 to configure the firewall settings.3. (optional) On the left column, selectAdvanced settings, and then go toInbound Rules > Windows Management Instrumentation(WMI-In).4. (optional) On theScopetab, selectAny IP addressin theRemote IP addressbox.
- Scan typeSelectChanges from last scanto only scan the changes compared to the last scan.SelectFull scanto perform a full scan.
- If theIP address rangeoption is selected, specify theStart IP addressandEnd IP address.Keep theUnlimited hopscheck box selected if you don't want to limit the number of hops. Clear the check box to enter the maximum number of hops.
- If theIP subnetoption is selected, specify theNetwork IP address,Subnet mask, andHost address range.
- LoginSpecify a login account. The account format varies for domain and local accounts.
- For domain accounts:domain\username
- For local accounts:Computer name\username
TIP: Ensure that the specified login account has the administrator access to each local computer. - PasswordSpecify the password for the account.
- Advanced SettingsClick the button to configure the following settings:
- Maximum scanning time [min]
- Device response timeout [msec]
- Node identification timeout [sec]
- Community string
- Host response timeout [msec]
- Software scanning mode
Provide Feedback